Onlangs gezocht

    Non-Latching Relays

    Relays are electrical switches that are operated by electrical impulses with the primary function to open and close a circuit, they can also be referred to as industrial switches. There are 2 main types available, latching and non–latching relays.

    How do non-latching relays work?

    Non-latching relays are in a normally closed (NC) position and will stay in this state without power. When power passes through the circuit, the relay switched to a normally open (NO) position by using an internal coil to generate a magnetic force, holding this NO position. Once the current is turned off, it returns to the NC position. This makes non-latching relays well suited to push-button applications like keyboards and micro-controller input buttons.

    What are non-latching relays used for?

    Non-latching relays are highly durable and versatile components, making their performance long lasting and suitable for use in a wide range of applications, such as:

    • Automotive engines
    • Household appliances
    • Industrial machinery
    • Medical equipment
    • Telecommunications equipment

    What is the difference between latching and non-latching relays?

    Both types of relays in similar in design and function, however, a significant difference between them is that a latching relay will remain in the last position it when it was last powered, whereas a non-latching goes back to its normal position. This makes each more type of relay suitable for different applications.

    Considerations when selecting a relay

    When choosing a relay, it is important to consider a number of specifications to ensure it is fit for purpose, some factors include:

    • Coil voltage - the required voltage to actuate the switching mechanism. If a voltage is too high this could damage the components, if it is too low then it will not actuate.
    • Contact configuration - This is the state the contacts are in without power. For example SPST, single pole single throw.
    • Contact material - the relay contacts are available in many materials that have certain properties. Common materials are gold, silver, tin oxide and nickel
    • Coil power - the amount of power (watts) the coil operates at. This must match the power in the circuit for correct function.
    • Coil resistance - the amount of resistance (ohms) in the circuit that the coil creates.
    Filters
    Sorteer op
    Pagina
    1
    van
    0
    per pagina
    Pagina
    1
    van
    0
    per pagina