MCBs

MCBs, or miniature circuit breakers, are a type of switch used to automatically turn off electrical circuits during abnormal conditions. MCBs often replace fuses in low voltage electrical circuits as they can be more reliable, much more sensitive and are resettable.

How an MCB Works

When continuous overcurrent flows through an MCB, a bimetallic strip is heated and causes it to bend. This bending of the bimetallic strip releases a mechanical latch opening the contacts and turning off the MCB, thereby stopping the current to flow in the circuit. To restart the flow of current the MCB must be manually turned on. This mechanism protects the MCB from faults arising due to overcurrent or overload and is intended to prevent the accidental overloading of the cable in a no-fault situation. The speed of the MCB tripping will vary with the degree of the overload. This is usually achieved by the use of a thermal device in the MCB. The second characteristic is the magnetic fault protection, which is intended to operate when the fault reaches a predetermined level and to trip the MCB within one-tenth of a second. The level of this magnetic trip gives the MCB its type characteristic.

MCBs are used to perform many functions such as local control switches, isolating switches against faults and overload protection devices for installation or specific equipment or appliances.

MCB Types

MCBs have three common types for circuit protection in residential, commercial and industrial applications. The use is classified by a type, which determines the tripping characteristics of the MCB:

Type B - trips between 3 and 5 times the load current

This type will trip instantly at a rate of three to five times its rated current. These are normally used for resistive or small inductive loads where switching surges are very small. Therefore, these are suitable for residential or light commercial installations.

Type C - trips between 5 and 10 times the full load current

This type will trip instantly at a rate of five to ten times its rated current. These are normally used for high inductive loads where switching surges are high such as small motors and fluorescent lighting. In such cases, type C MCBs are preferred to handle higher value of short circuit currents. Therefore, these are suitable for highly inductive commercial and industrial installations.

Type D - trips between 10 and 20 times the full load current

This type will trip instantly at a rate of ten to twenty-five times its rated current. These are normally used for very high inductive loads where high inrush current is very frequent. These are suitable for specific industrial and commercial applications. The common examples of such applications include x-ray machines, UPS systems, industrial welding equipment, large winding motors, etc.

How to select a suitable MCB for the application?

Focus on 3 main points to choose the right MCB for the electrical circuit

  1. Ampere rating
  2. Short circuit breaking capacity
  3. Application type

...
Lees meer Lees minder

Filters

1 - 7 van 7 producten worden weergegeven
Resultaten per pagina
Omschrijving Prijs Number of Poles Current Rating Model Number Range Series Tripping Characteristics Rated AC Voltage Rated DC Voltage Breaking Capacity Mounting Style Length Width Depth Application
RS-stocknr. 859-6149
Fabrikantnummer0830925
FabrikantPhoenix Contact
17,96 €
1 Box of 10
Box(es)
- - - - UM1-TM (3.5X12) - - - - - - - - -
RS-stocknr. 859-6127
Fabrikantnummer0830909
FabrikantPhoenix Contact
12,86 €
1 Box of 10
Box(es)
- - - - UM1-TM (6X12) - - - - - - - - -
RS-stocknr. 859-6105
Fabrikantnummer0830902
FabrikantPhoenix Contact
11,57 €
1 Box of 10
Box(es)
- - - - UM1-TMF (5X5) - - - - - - - - -
RS-stocknr. 859-6130
Fabrikantnummer0830924
FabrikantPhoenix Contact
11,57 €
1 Box of 10
Box(es)
- - - - UM1-TMF (8X5) - - - - - - - - -
RS-stocknr. 859-6136
Fabrikantnummer0830920
FabrikantPhoenix Contact
12,86 €
1 Box of 10
Box(es)
- - - - UM1-TM (8X12) - - - - - - - - -
RS-stocknr. 859-6108
Fabrikantnummer0830903
FabrikantPhoenix Contact
12,86 €
1 Box of 10
Box(es)
- - - - UM1-TM (6X10) - - - - - - - - -
RS-stocknr. 859-6102
Fabrikantnummer0830904
FabrikantPhoenix Contact
11,57 €
1 Box of 10
Box(es)
- - - - UM1-TMF (6X5) - - - - - - - - -